260130_LSS900100_eConfigure_KNX_SW

Creating Scenes without Using Templates

You can create custom scenes without using templates.


  1. Click New scene down on the left.

  2. Select your Link type.

    KNX scene: The KNX scenes are activated, a sensor device (e.g., a push button) sends a scene number. The actuator activates an output action stored at this scene number.

    NOTE: Wireless devices do not support KNX scenes.

    Central linking: The sensor (e.g., a push button) sends a value directly to one or many actuators (e.g., 95% for dimming).

  3. Fill in the scene name and your description (optional).

  4. Select None in the From template menu.

  5. Include devices and loads of your project in the scene.

  6. Click OK.

Your new custom scene appears in the list of scenes on the left.


In the next step, assign loads to your scene:

  1. Click your scene on the left select loads you want to add to your scene by clicking the connection point on the floor plan.

  2. Select your floor.

  3. On your project map, select the loads you want to include in your scene - click the black dot next to your load. After the black dot turns orange, your load becomes part of the scene.

  4. Go to the Parameters section on the top right and configure each load according to the function assigned to it:

    • Management of lighting intensity, rather than switching on/off

    • Opening/closing of roller shutters or specific level

    • You can enter thermoregulation (heating and cooling) by selecting the thermostat channel of the control devices (e.g., Multitouch Pro).

  5. The last step to complete the scene function is choosing the control device from which you activate the scene. To do this, select at least one (free) channel of the control device (e.g., Multitouch Pro, Pro Button, contact interfaces, push-buttons).


Maximum number of scenes per items:

  • Lighting and dimming – 5

  • Switch and socket loads – 5

  • Thermostats (except Multitouch) – 8

  • Multitouch – 4


NOTE: Some thermostats are not possible to be integrated into scenes (Altira, Unica).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.