260130_LSS900100_eConfigure_KNX_SW

ZigBee Devices Unpairing

To unpair your ZigBee device, do the following:

  1. In the UPLOAD tab, select your device in the list of configured devices on the right side of the UPLOAD tab.

  2. Click Reset the device.

  3. Follow the eConfigure KNX instructions for unpairing.

After unpairing, the device will appear back on the left side of the screen in the UPLOAD tab.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.