260130_LSS900100_eConfigure_KNX_SW

KNX Topology

The KNX Topology tab displays devices divided by location. Initially, this tab remains empty until you configure the actuators. Once the actuators are configured, all devices will be displayed in the KNX Topology tab, divided into segments and lines. eConfigure KNX automatically assigns a power supply to each segment based on the power consumption of the devices in that segment.


Configuration details

  • Lines and Devices: With eConfigure KNX Lite, you can use the main line of area one and three additional lines. Each line can be assigned up to 63 devices. eConfigure KNX automatically assigns the first 63 devices to line 1.1. Additional devices will remain on the left side for manual assignment (Devices not associated).

  • Segments: If you have more than 64 devices, distribute them into segments of the KNX bus. When you add a new segment, eConfigure KNX automatically adds a SpaceLogic KNX Bus Coupler as a repeater.


Device display

Devices are displayed as tiles with information on their name, location, and group address. You can:

  • Modify individual addresses:

    1. Click on your device tile.

    2. Fill in the numbers.

    3. Click OK.

  • Remove devices: Click × to remove devices.

  • Replace power supply: Click on the power supply and select the item from the list.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.