260130_LSS900100_eConfigure_KNX_SW

Installation Status

Warnings and errors are displayed in Installation status section.

If you click UPLOAD > Installation status, you can see a detailed list of the installation elements and descriptions of the problems.

  • Errors are problems that prevent the software from running.

  • Warnings are problems that do not prevent the software from running but may be forgotten on your part.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.