260130_LSS900100_eConfigure_KNX_SW

eConfigure KNX Lite Software

The eConfigure KNX software is a tool for designing, configuring, and maintaining the KNX building automation systems at different stages of the project:

  • Quotation

  • Commissioning

  • Maintenance

Software Availability

The eConfigure KNX Lite software is free to use. However, if you need to perform commissioning, you must purchase a dongle with a license.

Dongle License Requirements

Do I need a dongle license?

  • You do not need to purchase a dongle if you are not commissioning devices.

  • A dongle with a license is required to log in and download the software to your devices.

  • The dongle is available as LSS900100.

  • An initial version of the software is provided on the enclosed USB memory. After installation, an update tool will be available on your desktop.

Important Notes

  • eConfigure KNX does not replace professional trade knowledge. For example, basic knowledge of heating applications is recommended for installing heating management devices.

  • You do not need to be an expert in ETS to work with eConfigure KNX.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.