260130_LSS900100_eConfigure_KNX_SW

Floor

In the FLOOR tab, you can create a floor plan with rooms, add devices from the catalog and set their parameters.

You can also create and control scenes.

NOTE: The Undo function is not supported. Keep this in mind as you create your floor.

In the FLOOR tab, there are the following tools and areas:

  • The work area with a floor plan:


  • Toolbar:

    • Add floor

    • Select the room layout

    • Copy

    • Paste

    • Delete

    • Multiple selection
      (Click the icon > hold the left mouse button while moving over the floor plan and mark with a rectangle all the devices that you want to select.)

    • Search

    • Filter

    • View options

    • Help


  • CATALOG (Loads, Devices, Virtual Devices, Solutions)

  • SCENES module (Create/Control scenes)

  • PARAMETERS (select a device, load, or virtual devices and change their parameters)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.