260130_LSS900100_eConfigure_KNX_SW

Software Limitations

The eConfigure KNX software allows for the fast and easy implementation of KNX/ZigBee devices, but it has some limitations compared to the ETS software:

  • Limited Parameters:
    The parameters available in eConfigure KNX are fewer than those in ETS.

  • Functionality:
    Not all KNX functionalities are available in eConfigure KNX.

  • Project Requirements:
    Ensure that all the features needed for your project are available in eConfigure KNX.

  • Device Compatibility:
    You can find the list of compatible KNX/ZigBee devices within eConfigure KNX.

  • Project Size:
    eConfigure KNX
    is limited to projects with a maximum of 1000 KNX devices and 50 ZigBee devices.

  • Minimum Screen Resolution and Scaling Requirements:
    To ensure optimal performance and usability, eConfigure KNX requires a minimum screen resolution of 1366 x 768 pixels when using a 100% display scaling setting. For the best user experience, we recommend a resolution of 1920 x 1080 pixels, with a display scaling between 100% and 150%. Using resolutions or scaling settings below the minimum may result in interface elements not displaying correctly or reduced functionality.

  • Operating System Support: Only 64-bit (x64) versions of Windows are supported for ETS5 and ETS6.
    Supported operating systems:

    • Microsoft Windows 10 x64

    • Microsoft Windows 11 x64

    IMPORTANT: eConfigure KNX Lite cannot be installed on 32-bit versions of Windows 10.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.