260130_LSS900100_eConfigure_KNX_SW

Loads

Loads are all the non-communicating elements of the installation.

Each load is connected to an actuator of the Switchboard tab.

Loads are not compatible with all actuators. It is important to choose the right loads in the Floor tab.

In the automatic composition of actuators, each load is linked to a specific family of actuators and has its icon.

When you hover the cursor over the load icon, the parameters of the load appear.

Drop and drag loads directly into your floor plan and name them.


There are the following types of loads available:

Lighting area 10 A

Compatible with:

MTN6492xx (used in automatic composition < 2 ch)

MTN6705-0008 (used in automatic composition > 2 ch)

Switch area 16 A

Compatible with:

MTN647x93 (used in automatic composition)

Dimming area

Compatible with:

350 W: MTN6710-0102 (used in automatic composition), MTN649350, MTN649310

500 W: MTN649350 (used in automatic composition), MTN649310

1000 W: MTN649310 (used in automatic composition)

Group of ballasts 1 - 10 V

Compatible with:

MTN64xx91 (used in automatic composition)

Group of ballasts RGB DALI

Compatible with:

MTN6725-0101 SpaceLogic KNX Dali Gateway Pro (used in automatic composition)

Group of ballasts DALI (FW 1.x.x)

Compatible with:

MTN6725-0001 (used in automatic composition)

Group of sockets

Compatible with:

MTN647x93 (used in automatic composition)

Shutter/Blinds

Parameter 230 V

Compatible with:

350 W: MTN6710-0102

230 Vca: MTN6498xx (used in automatic composition)

24 Vcc: MTN6497xx (used in automatic composition)

230 Vca: MTN6705-0008 (used in automatic composition > 2 ch)

Floor heating area

Compatible with:

MTN6730-0002 (used in automatic composition)

Fan coil controller

Compatible with:

MTN645094 (used in automatic composition)

Binary input

Compatible with:

MTN644492 / MTN644592 (used in automatic composition)

MTN644892 / MTN644792 (used in automatic composition)

MTN644992 / MTN644692 (used in automatic composition)

NOTE:

If you want to remove a device/load already added to a Moment, remove the device/load group addresses from your Moment.

Find out more in chapter 18 Scenes, of your controller user guide here: https://www.se.com/eg/en/product/LSS100200/spacelynk-logic-controller/ or https://www.se.com/eg/en/product/LSS100100/wiser-for-knx-logic-controller/

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.