260130_LSS900100_eConfigure_KNX_SW

Generate Project in ETS

You transfer the eConfigure KNX Expert project to ETS as follows:

  1. In ETS, create and name your new project to which you want to transfer the data from eConfigure KNX Expert. Open your new project in ETS.

  2. In eConfigure KNX Expert, click Products at the top right of the screen.

  3. In the Bill of materials, click Generate project in ETS.


The data from eConfigure KNX Expert are transferred to your ETS project.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.