260130_LSS900100_eConfigure_KNX_SW

Shortcuts

While managing your project, you can use the following shortcuts:

Shortcut

Command

CTRL + C

Copy.

Select the device with the mouse, copy it by pressing CTRL + C. Then you can paste it somewhere else using CTRL + V.

CTRL + V

Paste.

The paste of an item is not immediate; it is necessary to position the item on the plan and click to validate the paste.

CTRL + A

Select all items on the floor or all text of a selected area.

CTRL + R

Draw the contours of a rectangular room.

CTRL + P

Draw the outline of a polygon room (max. 15 faces).

CTRL + S

Multiple selection modes.

ESC

Return to classic mode (from any mode).

CTRL + mouse wheel

Zoom in/out.

CTRL + N

Create solution

Click on the item on your floor plan, press CTRL + N, and fill in the parameters of the new solution.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.