260130_LSS900100_eConfigure_KNX_SW

Scenes

The scenes are combinations of actions triggered by a single command. You can create your scene from scratch or use scene templates. You can easily edit and delete your scenes in the Scene tab.

When creating a scene, you can only select the channels connected and compatible with the scenes.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.