260130_LSS900100_eConfigure_KNX_SW

Ethernet (IP Settings)

Set the IP configuration of the controller according to how the controller is connected to your computer.

Ask the user what type of IP protocol they prefer:

Static IP

Controller is directly connected to the computer via ethernet cable. (If you want to work with the controller, your computer has to be on the same IP network as the controller.)

Static IP is generally used in commercial buildings. Ask the IT specialist responsible and ask them about the settings.

DHCP (automatic)

Select this option if your controller is connected via a router.

DHCP is generally used in residential installation if you connect your controller to the DSL router of your end-user.


Take an IP training or contact the integrator for more details about the automatic and manual connection.

NOTE: After the commissioning, the controller is accessible via the IP address you enter here.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.