260130_LSS900100_eConfigure_KNX_SW

DALI Gateway Configuration

If you have a DALI Gateway in your installation, you need to assign the lights (ECGs) to DALI groups after the configuration of DALI Gateway. All the ECGs must be powered and connected to the DALI Gateway via the DALI bus.


In the list of commissioned devices on the right side of the screen in the UPLOAD tab, find the DALI gateway you want to configure and proceed as follows:

  1. Click Configure button in the device line > select one of the following options:

    • New installation:
      You start the new installation process. This includes searching for all lights and deleting the existing configuration.

    • Post installation:
      Post installation means maintaining the existing configuration (adding/removing lights) and searching for new lights.

    • Download configuration to download group configuration into the DALI Gateway and the ECGs.

      NOTE: No new lights are searched for. Only the configuration of already discovered lights will be downloaded.


  2. You can search for the right light to assign inside the Unassigned lights section.
    You can identify the light as follows: Right-click the light icon and select one of the following options:

    • Turn on: The light turns on

    • Start blinking: The light starts blinking.

      To turn off the light, right-click the light icon and click Stop blinking/Turn off.

  3. Drag and drop unassigned lights and assign them to groups. The changes are saved immediately to the DALI Gateway.

  4. Click Close.


DALI Gateway is configured.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.