260130_LSS900100_eConfigure_KNX_SW

Switchboard

The SWITCHBOARD tab is divided into three main areas:

  • Actuators: When the floor plan design is finished, the next step is to assign your loads to actuators. If only one switchboard per floor is required or one for the whole building, this can be done automatically. Otherwise you can do it manually or semi-automatic.

  • Controller: Adding a controller will allow you to access user interface, trends, schedules, Modbus and wireless devices.

  • KNX Topology: This tab displays devices divided by location.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.