260130_LSS900100_eConfigure_KNX_SW

Date & Time

In the DATE & TIME section, choose the time zone in which your controller is located.


If you change the time zone, you may lose energy data.

The time zone changes in some cases during a firmware reset/upgrade as shown in the following table:

Time zone updates

Time zone does not update

Upgrade/Reset controller firmware + replace configuration

Upgrade/Reset controller firmware + update configuration

Replace configuration

Update configuration

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.