260130_LSS900100_eConfigure_KNX_SW

Devices

In DIAGNOSTICS > ZigBee > Devices, you can view all paired devices and perform the following actions:

View Device Information

For each device, you can access detailed information including:

  • MAC address

  • Name

  • Manufacturer

  • Model

  • Firmware version

  • Battery level

  • Link quality

  • Update time

  • State

  • Actions

  • Location

View Device Configuration

To view the configuration of a device:

  • Click the Configure button or the configuration icon .

  • Configuration is available only for devices with a white background, indicating they are configured.

View Device Parameters

If parameters are available:

  • Click the Parameters button or the parameters icon .

  • Parameters can only be viewed for configured devices (white background).

Remove Devices

To remove a device from the network:

  • Click the delete icon at the end of the device line.

  • Confirm by clicking Yes.

Device Color Indicators

The background color of each device indicates its status:

  • White
    Device is configured.

  • Yellow
    Device is not configured.

  • Red
    Device has left the network.

  • Green
    Device is undergoing a firmware upgrade.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.