260130_LSS900100_eConfigure_KNX_SW

Logs

The network log is a real-time data set that records messages, commands, and communications related to network operations.

You can capture individual packets or groups of packets for purposes such as analysis, traffic monitoring, or troubleshooting.

The network log may include various types of information, such as:

  • Job time, step time, and data generated by user-defined routines

  • Operational data

  • Descriptions of unusual or unexpected events

You can export the log data as a .txt file and save it locally for further review or documentation.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.