260130_LSS900100_eConfigure_KNX_SW

Scan Bus Messages

To see the traffic of your network you can run the Scan Bus Messages feature:

Click DIAGNOSTICS tab > KNX > Scan Bus Messages > .

While scanning all the messages are monitored.

Each message provides information about:

  • Hour (sending time)

  • Service

  • Source address (of sending device)

  • Source name (device name)

  • Destination address (device group address)

  • Destination name

  • Info (value of the message – On, Off, Up, Down, percentage, etc.)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.