260130_LSS900100_eConfigure_KNX_SW

Diagnostics

The DIAGNOSTICS feature helps you to identify devices of your network and detect configuration inconsistencies. KNX and Zigbee devices are diagnosed separately.


The diagnostics tool provides three functions to identify a device:

  • Identify devices through bus monitoring

  • Check individual addresses

  • Identify all devices in programming mode


Diagnostics is useful, for example, in the following situations:

  • You want to upload your device, but the group address is already taken. You want to see which device is using this address so that you can upload the application to the right device.

  • You note that clicking the button does not turn on a lamp. You want to find this button in the eConfigure KNX project (as there are several buttons in the same room).

  • You suspect that a button is not connected to the right actuator. You want to identify the right actuator, to connect the button to this actuator.



The software guides you step by step through the entire diagnostics process.

You can also perform the diagnostics manually using the individual buttons in the lower half of the DIAGNOSTICS tab.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.