260130_LSS900100_eConfigure_KNX_SW

ZigBee Diagnostics

In the ZigBee device DIAGNOSTICS section, you can view the status of individual devices, access a list of logs, and monitor device activity in real time.

To start the diagnostics:

  1. Click DIAGNOSTICS > ZigBee > Connect.

  2. Select the desired tab: Devices, Logs, or Monitor.

Each tab provides specific insights:

  • Devices: Displays the current status and connectivity of each ZigBee device.

  • Logs: Shows a chronological list of recorded events and system messages.

  • Monitor: Offers a live view of device communication and activity.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.