260130_LSS900100_eConfigure_KNX_SW

About the Document

Document Scope

This user guide is designed to provide comprehensive instructions for using eConfigure KNX, primarily focusing on the Lite edition.

However, the features and functionalities described within apply to all versions of the software, including Expert and Expert Student. This ensures that users of the Expert and Expert Student versions can also benefit from the detailed guidance.

The specificities of the Expert and Expert Student editions are addressed in eConfigure KNX Expert chapter, allowing all users to follow the guide and apply the information to their respective software effectively.

Validity Note

This user guide is valid for all editions of eConfigure KNX version 3.0.0:

  • Lite

  • Expert

  • Expert Student

While the primary focus is on the Lite edition, the features and functionalities described herein are applicable across all editions.

Product Related Information

  • eConfigure KNX Lite Edition: The Lite edition is designed for users who need a straightforward and efficient tool for their KNX projects. It includes all the essential features required for basic configuration and management.

  • eConfigure KNX Expert Edition: The Expert edition offers advanced features and tools for professional users who require more sophisticated functionalities. These include enhanced configuration options, detailed diagnostics, and additional customization capabilities.

  • eConfigure KNX Expert Student Edition: The Expert Student edition is tailored for educational purposes. It provides students access to the full range of features at a reduced cost, making it ideal for learning and training in KNX technology.

General Cybersecurity Information

In recent years, the growing number of networked machines and production plants has seen a corresponding increase in the potential for cyber threats, such as unauthorized access, data breaches, and operational disruptions. You must, therefore, consider all possible cybersecurity measures to help protect assets and systems against such threats.

To help keep your Schneider Electric products secure and protected, it is in your best interest to implement the cybersecurity best practices as described in the Cybersecurity Best Practices document.

Schneider Electric provides additional information and assistance:

Product Related Cybersecurity Information

  • Use a VPN service to encrypt your internet traffic and hide your IP with a physical location.

  • Use secure protocol access HTTPS://IP:Port.

  • Do not use port forwarding to access a controller from the public Internet.

  • If your router supports a guest network or VLAN, it is preferable to locate your controller there.

  • Set up network security at the appropriate level.
    The security method is determined by the ability of other network elements (firewall, protection against viruses and malware threats).

  • Make sure your antivirus is updated.

  • Use the strongest Wi-Fi encryption available.

  • Turn on the User Account Control on Windows.

  • Use BitLocker to encrypt the Windows operating system drive.

  • Do not share your Windows account with another user.

  • Make sure all your passwords are uncrackable.


In case you find cyber security incidents or vulnerabilities, please go to https://www.se.com/ww/en/work/support/cybersecurity/security-notifications.jsp and contact us.

You can read more on system hardening here: https://www.se.com/ww/en/download/document/AN002_107/.


Software from Schneider Electric is digitally signed.

Verify the authenticity of the executable file from Schneider Electric before you run it as follows:

  1. Find the downloaded file in File explorer in your local storage.

  2. Right-click the file to display its properties.

  3. You can find the digital signature details in the Digital signatures tab of the Properties dialog.

If there is any problem or doubts, do not install the software and contact customer support.

Schneider Electric hereby disclaims any responsibility or liability for potential security vulnerabilities, software defects, or operational inconsistencies that may arise from the use of ETS (Engineering Tool Software) versions provided by KNX Association (knx.org). While eConfigure KNX is designed to interface with ETS for seamless integration and configuration of KNX systems, Schneider Electric neither develops nor maintains ETS software and therefore cannot guarantee its integrity, security, or compatibility across all versions. Users are advised to consult KNX Association for the latest updates, security advisories, and support related to ETS.

Available Languages of the Document

The document is available in these languages:

Related Documents

To find documents online, visit the Schneider Electric download center (www.se.com/ww/en/download/).

Secure Removal and Disposal

Before uninstalling eConfigure KNX:

  • Backup configurations: Export all project files and configuration data to a secure location.

To uninstall:

  • Use the standard Windows uninstallation process: Click Settings > Apps > Installed apps > select eConfigure KNX and eConfigure KNX Catalog > click Uninstall and follow the on-screen instructions.

After uninstallation:

  • Manually delete the following folders (if they still exist):

    • C:\Program Files (x86)\Schneider Electric\eConfigure KNX

    • C:\Users\<username>\AppData\Roaming\eConfigure

    • C:\ProgramData\eConfigure

  • Remove any shortcuts, registry entries, or scheduled tasks related to eConfigure KNX.

If migrating to a new system:

  • Export the configuration from the old system: Use the built-in export function to save project files.

  • Transfer the files securely using encrypted USB drives or secure file transfer protocols.

  • Install eConfigure KNX on the new device, import the configuration files, and verify integrity.

  • Delete the original files from the old system.

Information on Non-Inclusive or Insensitive Terminology

As a responsible, inclusive company, Schneider Electric is constantly updating its communications and products that contain non-inclusive or insensitive terminology. However, despite these efforts, our content may still contain terms that are deemed inappropriate by some customers.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.