260130_LSS900100_eConfigure_KNX_SW

Example 2: Heating Control (Valves)

Thermostat settings

Heating control: PI continuous control (valves)


You can change several parameters, but the thermostat is ready to control heating without further changes.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.