260130_LSS900100_eConfigure_KNX_SW

Identification by Individual Address

If you know the individual address of your device (it is visible in the SWITCHBOARD > KNX topology or the UPLOAD tab), you may want to identify your device by typing its address.


If a device is found after you typed its address, turn on/off the programming LED of your device, so that you can locate it.

If there is no device at this individual address, run the Scan bus devices feature which may help you to find it.



Some devices may be detected but not recognized:

Those are labeled as Unknown device. They have probably been uploaded from another project in eConfigure KNX, or you have made significant changes in your project since you uploaded this device for the last time.

We recommend you reset such device and re-upload it so that it is updated.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.