260130_LSS900100_eConfigure_KNX_SW

Identification by Programming Button

Most devices have a programming button, which turns on (or off) a programming LED.


If you want to identify your device with its programming button, do the following:

  • Press the programming button of your device > click Start scan.

By default, detection starts on line 1.1.


If you want to look for a device on another line, click Show advanced parameter > type the number of the line to scan > click Start scan.

All the devices with their programming LED on display on the screen.


Press the programming button of the devices you do not want to identify to turn off their programming LED.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.