260130_LSS900100_eConfigure_KNX_SW

General Information

In the GENERAL INFORMATION section, select/fill in the following information about your controller:

  • Controller Type

  • Name: Name your controller. Once the name has been changed and the controller restarted, select the new interface in the UPLOAD tab.

  • Language: Set the language of your controler´s user interface.

  • Admin password: A password change is required if it does not meet the security requirements.

    Password complexity requirements:

    • The length between 8 – 32 characters

    • At least one uppercase letter

    • At least one lowercase letter

    • At least one digit (0 – 9)

    • European languages letters (A – Z with diacritics, sharp S, Greek and Cyrillic characters)

    The admin password will be changed on the controller during the next upload.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.