260130_LSS900100_eConfigure_KNX_SW

Upload

Once you have finished the floor plan and switchboards settings, you can move to the UPLOAD tab.

The UPLOAD tab is used to download the configured programs into the KNX devices. It also provides essential information and tools for finalizing the installation, including:

  • Installation status:
    Shows errors and warnings from the FLOOR and SWITCHBOARD tabs. Click Installation status to see an overview.

  • Devices to configure/Devices configured:
    On the left side of the screen, you see the devices that still need to be configured. On the right side, you see the list of devices that have already been configured.

  • Device programming:
    You can select devices and initiate the upload process by clicking the arrow button in the center of the screen. If a device is not yet addressed, press its programming button to assign an individual address.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.