260130_LSS900100_eConfigure_KNX_SW

ZigBee Devices

It is also possible to manage ZigBee devices in eConfigure KNX. In order to pair them with the controller, you have to connect your controller to the SpaceLogic KNX Hybrid module.

eConfigure KNX automatically installs the Hybrid plugin.

ZigBee devices support only one group address. If you connect several ZigBee devices to one switching device, a scheduler, or a central command, you cannot control the ZigBee devices separately.

Example:

Channel 1 of Avatar dimmer 1G and channel 1 of Avatar dimmer 2G are connected to the free locate switch. If you control one dimmer from the Touch application, the other dimmer reacts simultaneously.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.