260130_LSS900100_eConfigure_KNX_SW

Identification by Using the Device

If your device programming button is difficult to be accessed, you can identify your device by using it. This tool can detect unexpected messages on the bus (by detectors for example).

The detection process has to be running (visible on the bottom of the screen).

  • Trigger the device you want to identify, so that it sends messages to the bus (for example, click the button of a push-button or trigger the presence detector).

  • With the button Ignore this device, you can ignore any new message sent by this device during the detection process.

  • If you want to detect again a device you have ignored, click Show ignored devices: X (X = the number of ignored devices) > click Detect this device again.

  • If you want to ignore all devices except the one you wanted to identify, click Keep only this device.


Your device may be undetected because it did not send any message to the bus. You need to identify your device through the programming button or its address.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.