260130_LSS900100_eConfigure_KNX_SW

Controller Commissioning

If your installation includes a logical controller, you have to commission it using the UPLOAD tab.

Follow these steps to commission the controller:

  1. Locate and select the controller:

    • In the left section of the UPLOAD tab, find and click on the controller device.

  2. Set up controller access:

    • Click Select controller access at the bottom left corner of the screen.

    • First, configure the Default access type. (See the section Access Type Default for more details.)

  3. Configure User-defined access type:

    • After setting up the default access, proceed to configure the User-defined access type. (See the section Access Type User-defined for more information.)

Use the Remote access type to commission a controller via a secure remote configuration interface as described in the chapter Remote Configuration Interface of the SpaceLogic KNX Remote user guide.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.