Access Type Remote
The Remote access type in eConfigure KNX allows users to commission and configure KNX controllers that are not on the same local network. It is designed for secure, remote access using the SpaceLogic KNX Remote service.
For full setup instructions, refer to the SpaceLogic KNX Remote user guide.
Why Use Remote Access
Remote access is especially useful for:
-
Commissioning from anywhere – configure controllers via internet.
-
Diagnostics and updates – troubleshoot without traveling.
-
Secure access – reach controllers in restricted or distant locations.
-
Centralized management – handle multiple installations from one interface.
-
Remote parameterization – update Touch visualization or configure ZigBee devices
How It Works
To use Remote access, the following conditions must be met:
-
The controller supports SpaceLogic KNX Remote access.
-
A WireGuard VPN tunnel (Remote Configuration Access) must be granted by the controller owner before selecting Remote access type in eConfigure KNX.
-
The controller connects to the KNX bus and LAN via the IP interface.
-
In the UPLOAD tab, go to Select controller access > Access type > Remote.

-
The system automatically uses the IP address from the active VPN – no manual IP entry needed.
-
Once connected, users can upload configurations and perform remote parameterization just like in local modes.
Integration with SpaceLogic KNX Remote
The Remote access type relies on the Remote Configuration Interface, which becomes available when:
-
The controller is paired with a user account via the Wiser KNX mobile app or the Management plugin.
-
A valid SpaceLogic KNX Remote subscription is assigned to the controller.
-
Open SpaceLogic KNX Remote and connect to the controller you want to parameterize.
-
The Cloud Connector is enabled on the controller to establish a secure VPN tunnel.
Once connected, the configuration IP address is displayed in the SpaceLogic KNX Remote interface and used by eConfigure KNX to establish the remote session.
Important
-
Ensure the controller is properly configured for remote access.
-
The controller owner must grant Remote Configuration Access.
-
Your firewall must allow communication over the required ports (e.g., 3671 for KNXnet/IP).