260130_LSS900100_eConfigure_KNX_SW

eConfigure KNX Expert

eConfigure KNX Expert software is a plugin in ETS. eConfigure KNX Expert has all the features and appearance of the Lite version.

Compared to eConfigure KNX Lite, there is more to do with eConfigure KNX Expert.

You can:

  • Create your own devices.

  • Export your project to ETS.

  • In KNX topology tab, you can work with an unlimited number of areas and lines (max. 4 lines and 1 area in eConfigure KNX Lite).

NOTE: You can only use the eConfigure KNX Expert plugin with ETS Professional.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.