260130_LSS900100_eConfigure_KNX_SW

Remote Connection Using Direct Connection and Port Forwarding (Unsecured)

NOTE: Port-forwarding is an unsecured connection method. Anyone can connect to your network because a username and password are not required. It is recommended to use VPN connection instead.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.