260130_LSS900100_eConfigure_KNX_SW

ZigBee Devices Pairing

To integrate your ZigBee devices with the SpaceLogic KNX Hybrid application on your controller, follow these steps:

  1. Device selection:

    • Navigate to CATALOG > Devices.

    • Select the ZigBee devices you want to add to your floorplan.

  2. Room placement:

    • Drag and drop the selected devices into their respective rooms.

    • Link them with your installation (Channels and Links).

    • Configure their parameters in the Parameters tab (Parameters).

    NOTE: Safety ZigBee devices (such as alarms, water leakage sensors, and door/window sensors) automatically trigger each other via a separate IF network. No additional linking is required for these safety devices.
  3. Device pairing:

    • Go to the UPLOAD tab.

    • Choose the specific device you want to pair.

    • Click the arrow in the middle.

    • Follow the wizard steps.

    • If your device is not detected within 30 seconds, reset it (you can find the instructions in the wizard).

  4. Completion:

    • Click Close.

    • Once pairing is complete, the device will appear in the list on the right side of the screen.


NOTE: Be aware that initial pairing attempts may not always succeed. If you encounter issues, try again.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.