260130_LSS900100_eConfigure_KNX_SW

Creating Scenes from Templates

eConfigure KNX offers 10 scene templates that you can further customize.

Click New scene > fill in the scene name and its description > select your template from the following options:

Name

Function

Leave the building

  • Close blinds

  • Turn off lights

Enter the building

  • Open blinds

Light off building

  • Turn off lights

Light on building

  • Turn on lights

    In the case of adjustable lights, bring the intensity to 100%.

Light off floor

  • Turn off lights

Light on floor

  • Turn on lights

    In the case of adjustable lights, bring the intensity to 100%.

Blind down building

  • Close blinds

Blind up building

  • Open blinds

Blind down floor

  • Close blinds

Blind up floor

  • Open blinds

You cannot include the DALI lights of your project in scenes.

However, it is still possible to create group commands involving DALI lights. You must carry out this function by connecting DALI lights to a channel of a control device (for example, push buttons) and use the Set value function (between 0% and 100%). Then all the lights connected to the channel will turn on to the set intensity at the press of the corresponding button.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.