260130_LSS900100_eConfigure_KNX_SW

Hide, Show, Filter, Zoom

In this mode, it is possible to select either a device or a load and view links related only to this item. This comes in handy when you are checking the installation.

Click and filter your links. Tick the function category of links you want to display:

  • Lighting

  • Blind

  • HVAC

  • Socket

  • Other


You can zoom in and out of your map in two ways:

  • Use CTRL + the mouse wheel.

  • Click > adjust the zoom (or image and link opacity)


You can search for objects in your plan by name. Type the search term in the search box.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?