260130_LSS900100_eConfigure_KNX_SW

Firmware Upgrade

In the FIRMWARE UPGRADE section, you can enable the automatic upgrade of the controller firmware.
If you enable the automatic update of the controller firmware, eConfigure KNX Lite will always update the controller firmware to the latest available version.

To allow controller firmware upgrade, check Allow controller firmware upgrade.

After the controller firmware upgrade the controller will be used in the production environment. Leave this option disabled if you are involved in product testing and continue using the pre-production environment.

NOTE: It is highly recommended to enable this feature.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.