260130_LSS900100_eConfigure_KNX_SW

Devices

The term devices means all the communicating devices that can be installed in the rooms:

  • KNX

  • Wireless


The devices are represented by icons. When you hover the cursor over the device icon, the parameters of the device appear.

You can use filters to display a selection of devices. Filtering categories and ranges (for push buttons) is possible.

You can drag and drop devices directly to your floor plan.


There are the following types of devices available:

Push buttons

Push buttons control the installation. They are available with 2, 4, 6, and 8 keys.

Some devices have an IR function to allow the remote-control infrared commands.

Push button interfaces

Push button interfaces control the installation. They are installed in the installation box behind all kinds of conventional push buttons. They can have 2 or 4 inputs.

Push button Pro T

Push button Pro controls the installation. You can set the number of keys (1, 2, 3 or 4). It allows an adaptation on site without changing the reference.

Thermostat

Thermostats allow heating area management and/or a cooling zone setting.

Some thermostats have buttons, whose functions are the same as the push buttons.

Multitouch

The multitouch controls the installation (lighting, shutters, ...) as well as heating and cooling. It has a built-in touchscreen.

Presence/Movement detectors

You can set monitoring of presence or movement with the presence/movement detectors.

Some of them allow the lighting regulation.

Various sensors

CO2, humidity, temperature – indoor or outdoor (weather station). It is possible to back up the information in real time and to automate specific functions of the building.

Valve drive

The valve drive controls the valves of the water heating system.

Actuators embedded

Built-in actuators manage loads closing. They are used in projects where the electric cables do not allow installation of KNX components.

NOTE:

If you want to remove a device/load already added to a Moment, remove the device/load group addresses from your Moment.

Find out more in chapter 18 Scenes, of your controller user guide here: https://www.se.com/eg/en/product/LSS100200/spacelynk-logic-controller/ or https://www.se.com/eg/en/product/LSS100100/wiser-for-knx-logic-controller/

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.