260130_LSS900100_eConfigure_KNX_SW

Monitor

The Monitor function allows you to track device activity within the network, along with the values reported by each device.

The following information is displayed:

  • Number
    Sequential identifier of the entry

  • Time
    Timestamp of the recorded activity

  • Type
    Type of message or event

  • Link quality
    Signal strength or quality of the connection

  • Address
    Device network address

  • Name
    Device name

  • Model
    Device model identifier

  • Cluster
    Communication cluster used

  • Group
    Group ID, if applicable

  • Action
    Type of action performed or triggered

  • Data
    Data payload or reported value

You can export the monitored data as a .csv file and save it locally for further analysis or record-keeping.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.