260130_LSS900100_eConfigure_KNX_SW

Creating Reports from Your BOM

At any stage of your project, you can generate various reports from the Bill of Materials (Bill of Materials (BOM)).

To do this, follow these steps:

  1. Click .

  2. Select Export reports and lists.

Once the reports and lists are generated, you can save them as a *zip file to your local storage.

The following reports are included in the exported *.zip file:

  • Bill of material

  • Installation/customer report

  • User report

  • Floor plans

  • *.esf file with group addresses

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.