260130_LSS900100_eConfigure_KNX_SW

Identify Devices

In the DIAGNOSTICS tab > KNX, you can identify a device on your network with Identify a device function.

There are three ways how to do it:

  • Press the programming button.

  • Use the device to be identified.

  • Type the device individual address (click Show advanced identification feature).

Follow the step-by-step guide which will guide you in diagnosing link issues.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.