260130_LSS900100_eConfigure_KNX_SW

Manage and Edit Group Addresses

You can manage and edit group addresses in your project.

Manage group addresses as follows:

  1. Select the right floor and your device.

  2. Click the device connection line.

  3. On the right side of the screen, click Manage group addresses.

  4. In the Manage link group addresses, click the Compute links. This feature analyses the datapoints in the link and generates the appropriate group addresses for each datapoint.

  5. If you want to change the group address (define your own) of your device, type the new address into Forced address column click Close.

Edit project addresses as follows:

  1. On the right side of the Floor tab, click Edit project addresses.

  2. A list of all group addresses of your project opens where you can:

    • Force supervision addresses (The supervision address is an address that is used to control the device directly from the Touch application. The controller itself assigns the supervision address to individual devices.)

    • Reset forced addresses (remove forced addresses).

    • Delete all addresses


Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.