260130_LSS900100_eConfigure_KNX_SW

Adding a Controller to Your Installation

The controllers can add several functionalities to your installation and the users:

  • Visualization

  • Schedulers

  • Modbus, wireless, IHC devices integration

  • Energy monitoring

  • Trends

  • Advanced logic


With the controller, you configure devices and generate a graphical interface for users to control the installation from their smartphone or tablet.

For Wiser for KNX there is the Wiser KNX app available on Google Play and Apple Store (Mobile App).



To add a controller, do the following:

  1. Go to SWITCHBOARD > Controller > Add a controller.

  2. In the SWITCHBOARD > Controller tab, you can then set the detailed parameters of your controller in the following sections:

    • GENERAL INFORMATION

    • MOBILE APP

    • FIRMWARE UPGRADE

    • DATE & TIME

    • ETHERNET

    • KNX

    • HYBRID CONFIGURATION

    • END USER ACCOUNT


The GUI configuration is automatic.

You can make changes directly in the configuration of the controller interface.

Reprogramming with eConfigure KNX Lite may result in the loss of information if you select Replace in the UPLOAD tab > Select controller access > Configuration.


It is recommended to save a copy of your complete project and your visualization in the controller. Information on how to do it is available in the product guide of the Wiser for KNX and spaceLYnk controllers.

Follow the user guides on how to configure and use Wiser for KNX and spaceLYnk controllers or look for the online tutorials at https://community.se.com/.


Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.