260130_LSS900100_eConfigure_KNX_SW

Hybrid Configuration

If your installation contains wireless devices, get the ZigBee network configuration data from your Hybrid module in the HYBRID CONFIGURATION tab:

  1. Go to SWITCHBOARD > Controller > click HYBRID CONFIGURATION > Get data.



  2. If you need to change the obtained data (for example, change the channel), make changes in the form and click Set data.

NOTE: Changing the network configuration requires the devices to be paired again. Changing the channel without changing the PAN ID may prevent creation of a new network. Commission your controller before you change the Network key.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.