260130_LSS900100_eConfigure_KNX_SW

Example 3: Movement Detection (External)

In this example, the settings of the detector are directly set. The user changes the timer, sensitivity, and range right on the device.

You can change several parameters, but the detector is ready to control lighting without further changes.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.