260130_LSS900100_eConfigure_KNX_SW

Scan Bus Devices

With the Scan Bus Devices function, you can scan for devices that are physically configured on lines.

In DIAGNOSTICS tab > KNX, click Scan Bus Devices and select the line you want to scan. The lines correspond to the lines defined in SWITCHBOARD > KNX Topology.

Devices are sorted into three columns according to the scan result:

  • Found devices

  • Missing devices

  • Unknown devices

If a device does not appear anywhere, you may look for it in SWITCHBOARD > KNX Topology, whether it is configured on the correct line according to your electrical wiring.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.