Advanced Tab

The Advanced tab contains other technical configurations. The available functions vary depending on the stage of your implementation. Some of these configurations are used during implementation then turned off at project initialization.

For example, the application requires an integration with your Work Management System (WMS) to create designs. Before that integration is complete, the Advanced tab contains a Work Requester function as a short-term method for creating designs. When the integration is ready, the temporary Work Requester is turned off. Similarly, the Customer WMS function is another temporary solution used to track a work request from assignment through build and completion. This stand-in for your WMS includes options to create sessions, push to the GIS, delete work requests, and reopen closed work requests. Both Work Requester and Customer WMS functions include the information tag, “For Testing Only”, as a reminder that these are temporary and allow the implementation team to test the workflows before integration with your WMS is complete.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?