Dead Letters Search

Type search criteria to make it easier to find existing dead letter messages. The search leverages a query end point in the Azure Service Bus messaging service to perform server-side queries of dead letter messages.

You can search by the following parameters:

  • SessionId

  • ExceptionMessage Details

  • MessageBody Details

  • MessageType Fields

The search queries both Topics and Queues at the same time (see the first image below for an example).

IMPORTANT: Search by one parameter at a time. Do not combine parameters within the same search. For example, do not copy and paste a SessionId and part of the ExceptionMessage in the same search. Combining the parameters produces no results, but searching them separately produces results.

For example, a part of the Exception Details were queried in the following image, and the search results are filtered to only those Topics and Queues matching those details:


As another example, a MessageType was queried in the following image, and the search results are filtered to only those messages matching that MessageType:


To facilitate searching across all four parameters listed above, the search string typed in the search bar is converted to the query below before it is sent to the server. Using the example above searching for “DesignCreated,” the query would appear like the following:

select * from c where c.messageMetadata.SessionId ='DesignCreated'
OR CONTAINS(LOWER(c.messageMetadata.Properties.ExceptionMessage),LOWER('DesignCreated'))
OR CONTAINS(LOWER(c.messageBody),LOWER('DesignCreated'))
OR CONTAINS(LOWER(c.messageMetadata.Properties.MessageType),LOWER('DesignCreated'))

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?