Compatible Unit

This tab provides information about the CUs in your system, and it helps you maintain their attributes.

You can perform the following actions:

  • Click the Add button to add a new CU or add CU Attributes to an existing CU.

  • Click the Edit button to either edit the Related Equipment Specification or change the Available Work Functions.

  • Click Copy CU as a first step toward modifying and creating a new CU.

  • Click Delete to delete a CU.

IMPORTANT: After making changes, always update the Catalog Cache.

For more information about the relationship between CUs and Equipment Specifications, see the topic Relate a CU to an Equipment Specification.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?