Firewall Rules for Ports

Inbound and outbound rules for local ports are necessary for domains outside your server to access your ArcGIS Services. The local ports 6443, 6080, 443, and 80 need to be open to intra-network traffic.

Using Windows Defender Firewall, create both the inbound and outbound rules for these ports with the following configurations:

  • Rule Type: Port

  • TCP or UDP: TCP

  • Specific Local Ports: 6443, 6080, 443, 80

  • Action Taken: allow the connection

  • When Does the Rule Apply: check Domain and Private; uncheck Public

  • Name: provide a descriptive name you and other company administrators would understand


QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?