Annotation in Reference Views

Designer XI supports annotation in a Reference View.

The key part is you must choose the annotation with “Annotation Layer” as its type. The application does not support annotation with “Annotation SubLayer” as its type.

TIP: When choosing layers to create the Reference View, pay attention to the numbers in parentheses. The numbers are the layer IDs from the underlying published map service. In this manner, you can double-check you are choosing the correct annotation layer, especially if an Annotation SubLayer happens to be named the same as an Annotation Layer.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?